Encoder Emulation
RON TO PROVIDE TEXT.
| Element | Property | Description | Parameter | |
|---|---|---|---|---|
| Encoder Emulation Source |
|
Feedback source |
This parameter sets the position source used to drive the EEO generator. 1 – Feedback 1 3 – Feedback 3 4 – Feedback 4 5 – Feedback 5 |
|
| Configure Zero Pulse |
|
Zero Pulse Mode - Once per revolution | This parameter sets the position within each revolution where the Z pulse will be generated, when the one Z pulse per rev mode is selected (EEO#.ZMODE 0) | EEO#.ZOFFSET |
| Zero Pulse Mode - Absolute position | This parameter sets the position of the Z pulse when the absolute Z pulse mode is selected (EEO#.ZMODE 1). | EEO#.ZP | ||
| Encoder Emulation Output Generator |
|
Mode |
This parameter specifies the type of output waveform an EEO generator will create. 0 – A Quad B 1 – CW/CCW 2 – Step/Direction |
EEO#.MODE |
| Lines | 1.000 | EEO#.LINES | ||
| Pulse Width | 4.0800000 | EEO#.PULSEWIDTH | ||
| X23 |
|
Shows feedback and selecting will take you to the Hardware Configuration. |